Search FAQs
Is SoMachine V4.1 SP2 compatible with Windows 10?
Issue:
SoMachine V4.1 SP2 windows compatibility
Product Line:
SoMachine
Resolution:
SoMachine V4.1 SP2 supports Windows 7, 32 and 64 bit, as well as Windows 8.1, 32 and 64 bits only.
SoMachine V4.2 supports Windows10.
SoMachine V4.1 SP2 windows compatibility
Product Line:
SoMachine
Resolution:
SoMachine V4.1 SP2 supports Windows 7, 32 and 64 bit, as well as Windows 8.1, 32 and 64 bits only.
SoMachine V4.2 supports Windows10.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: