Issue:
ATV312 set up configuration to run upon power up and ramp up to full speed (60 hz).
Product Line:
Altivar 312, ATV312
Environment:
N/A
Cause:
N/A
Resolution:
Go into I-0- menu.
Set TCC to 2C.
Set TCT to LEL.
Go into SET- menu.
Set LSP to value desired in hz. For example, 60 hz is full speed.
Once programming is complete and drive powered down apply jumper to LI1 and +24V for run command.
Note: Drive will run motor as soon as power is applied to the drive with this configuration.
“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Released for:Schneider Electric Saudi Arabia