Search FAQs
How is the OPR parameter scaled on the ATV71 series drive?
Issue:
Scaling the Analog Output when using Output Power on an ATV61/71.
Product Line:
ATV61/ATV71
Environment:
All models, All serial numbers
Cause:
N/A
Resolution:
The output power (OPR) function is scaled between 0 and 2.5X the NPR (Rated motor power) setting under menu 1.1 (Simply Start). This parameter should be set to match the horsepower or KW rating of your motor in order for the output scaling to be accurate.
Scaling the Analog Output when using Output Power on an ATV61/71.
Product Line:
ATV61/ATV71
Environment:
All models, All serial numbers
Cause:
N/A
Resolution:
The output power (OPR) function is scaled between 0 and 2.5X the NPR (Rated motor power) setting under menu 1.1 (Simply Start). This parameter should be set to match the horsepower or KW rating of your motor in order for the output scaling to be accurate.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: