{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is there a way to read Mains Voltage on ATV212 over Modbus?
Issue:
Reading Mains Voltage on ATV212 over Modbus.

Product Line:
ATV212, Altivar 212, S-Flex

Environment:
All

Cause:
N/A

Resolution:
With the parameter FE04 (Modbus address = 65028) you can read the Mains Voltage.
This value is in percentage of the drive Rated Voltage (200V or 400V). For example with an ATV212…N4, FE04 = 10570 or 105.7% of 400V, which give 423V.

Schneider Electric Saudi Arabia