{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is 140NOE77110 module compatible with 140CPU67160 SV3.3?
Question:
Is 140NOE77110 module compatible with 140CPU67160 SV3.3?

Answer:
No. Since 140NOE77110 has been obsolete for many years, it was not involved in the V&V test with latest Quantum CPU firmware.
Our recommendation is NOT to use the 140NOE77110 but rather upgrade to the 140NOE771x1.

Schneider Electric Saudi Arabia