{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the Anti-Jam function on the Altivar 6xx Process drive?

Issue:
Anti-Jam function on the Altivar 6xx Process drive.

Product Line:
ATV6xx

Environment:
All serial numbers for ATV6xx

Cause:
N/A

Resolution:
Clogging substances can damage the pump.
This function allows manually or automatically executing forward & reverse pump rotations cycles to unclog.
It may also help to clear a blocked impeller, pipe, or valve at downstream location.
This should increase he efficiency of the system as well as the pump life time.

Schneider Electric Saudi Arabia

Explore more
Range:
Altivar Process ATV600
Explore more
Range:
Altivar Process ATV600
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.