Search FAQs
What are the dc power consumption values (110V dc) & mode of supply (permanent, short time, starting) for SF circuit breakers used in SM6-24?
Attached pages gives the power consumption of different auxiliary devices used with SF circuit breakers.
Information summarized below in reference to attached simplified wiring diagram for 110V dc power supply:
Information summarized below in reference to attached simplified wiring diagram for 110V dc power supply:
Type of auxiliary device | Power consumption (W) @ 110Vdc | Mode of supply/average duration | Re-occurrence |
Shunt closing release | 50W | short time/50ms | each closing cycle (according to application) |
Shunt opening release | 50W | short time/70ms | each opening cycle (according to application) |
Under voltage release |
| Continuous (10W) | Continuous |
Electrical motor with gearing | 380W | short time/15s | each closing cycle (re-arming of the closing spring), according to switching cycles/application |
Released for:Schneider Electric Saudi Arabia
Attachment(s)
Explore more
Range:
Explore more
Range: