Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
How to change the node name of a M241 and M251 with an SD card?
Issue:
How to change the default node name of a SoMachine / Machine Expert controller via an SD card

Product line:
M241
M251

Environment:
SoMachine 4.3
EcoStruxture Machine Expert

Resolution:
1. In SoMachine or Machine Expert/ Logic Builder go to Project / Mass Storage (USB or SDCard) in the main menu
2. Click on Add new ( + yellow sign)
3. Click on Choose a command and select SetNodeName
4. Enter the desired node name in the Device name field
5. Click on Generate and select your SD card or a place where to generate the files that will be later moved to the SD card

Notes:
- The method for this FAQ was verified with SoMachine 4.1 SP2, SoMachine 4.2, SoMachine 4.3, Machine Expert 1.2, Machine Expert 2.0
 - The node name can also be change when online with your controller by going to Device window / MyController / Communication settings tab. There right-click on your controller and select "Change device name..." to change the NodeName
 
 
If this FAQ did not solve your issue, you can chat with us at  chat with us  or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
 
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: