{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What keypad is compatible with the Altivar 320?
Issue:
Keypad compatibility with the Altivar 320.

Product Line:
Altivar 320

Environment:
All serial numbers for Altivar 320

Cause:
N/A

Resolution:
The Altivar 320 drive is compatible with the list of keypads:
  • VW3A1111 (Altivar Process Drive keypad)
  • VW3A1101 (Altivar 61/71)
  • VW3A1006 (ATV312/32 keypad - IP54)
  • VW3A1007 (ATV312/32 keypad - IP65)
The Altivar Process keypad requires mounting kit VW3A1112 (provides IP65).
The ATV61/71 keypad requires mounting kit VW3A1102 (provides for IP54, add VW3A1103 for IP65).

Cables must be ordered separately
  • VW3A1104R10 - 1 Meter Cable
  • VW3A1104R30 - 3 Meter Cable
  • VW3A1104R50 - 5 Meter Cable
  • VW3A1104R100 - 10 Meter Cable

Schneider Electric Saudi Arabia