{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to program an ATV630 (Process) drive to use the keypad for start/stop and AI1 for 4-20mA speed reference.
Issue:
ATV630 (Process) drive set up with keypad as start/stop and AI1 as 4-20mA speed reference.

Product Line:
Altivar ATV630

Environment:
All

Cause:
Programming

Resolution:
From main menu, go into to menu 5 (complete settings).
Scroll down to menu 5.5 menu (Command and reference) and press OK.
Set Ref Freq 1 config to AI1.
Set control mode to separate.
Set Cmd channel 1 to HMI.
ESC back to Complete settings menu.
Scroll down to menu 5.11 Inputs/Outputs menu.
Select AI/AQ tab.
Enter on AI1 configuration.
Set analog input type to current.
Set AI1 min value to 4mA.
Set AI1 max value to 20mA.

Schneider Electric Saudi Arabia