{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How configure VMWare in mode NAT and SoMachine for M251 communication via ETH 2 port
Use the following method with the VMWare configured in NAT mode:

1. Configure SoMachine the communication via "active path":

2.In the Communication Settings window , add a gateway and use the IP address of the
physique PC.

3.Select the new gateway and  Scan it

4. Now you can connect to the M251

Schneider Electric Saudi Arabia