Search FAQs
How to establish an EthIP communication when T->O transfert format is 32bitRunIdle
1. Import the Slave Eds File in SoMachine
2. Add the device in the Industrial Ethernet Manager
3. Add a Generic connection
4. Skip in the application the first 2 %IW in the Ethernet IP I/O Mapping
The first two %IW will show the status of the Slave. Customer will find the input values from the third %IW.
2. Add the device in the Industrial Ethernet Manager
3. Add a Generic connection
4. Skip in the application the first 2 %IW in the Ethernet IP I/O Mapping
The first two %IW will show the status of the Slave. Customer will find the input values from the third %IW.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: