{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the difference between UA and BA controllers used in Source change over system of NSX MCCB in the point of Load Shedding?
- For the Source change over system using MCCB of type NSX, in order to perform Load shedding and re-connection of on non priority loads,

This function is supported when using the Controller UA while it is not supported in the BA controller

Schneider Electric Saudi Arabia