{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the Trip unit of type TMD or TMG used with NSX MCCB protects against Ground Faults ?
- The TMD or TMG Thermal magnetic trip units that are used only with MCCB NSX of frame sizes 100-160-250 A are used only for Overload and short circuit protection and not ground fault protection.

- For ground fault protection, you can use:

1- Micrologic 6.2 (A/E) with NSX 100-160-250 A

2 -Micrologic 6.3 (A/E) with NSX 400-630 A

Schneider Electric Saudi Arabia