{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the dimensions of the 150 hp ATV660 drive with a harmonics filter?
Issue:
Looking for the dimensions of the 150 hp ATV660 drive with a harmonics filter.

Product Line:
ATV660

Environment:
All

Cause:
Looking for enclosure dimensions for ATV660 with harmonic filter.

Resolution:
Attached is the PDF with the drive dimensions for 150HP enclosure with harmonic filter built in.

Schneider Electric Saudi Arabia

Attachment(s)
CR-778256.pdfHarmonic enclosure dimensions.pdf [180.7 KB]