{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to solved library registration issue on SoMachine V4.1 / V4.2
Fact:  If you install SoMachine Basic V1.5 on a PC with SoMachine V4.x you are no longer able to register  the solution libraries (Packaging Library) direct from the SoMachine message window.

Reason: The License Manager V1.9.4.1 which are installed by the SoMachine Basic V1.5 setup routine is not compatible with SoMachine V4.x

Solution:
  • uninstall the new License Manager V1.9.4.1 manually, by using the windows Control Panel
  • reinstall the old License Manager V1.6 from SoMachine 4.2 DVD

Schneider Electric Saudi Arabia