{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the maximum customer cable size that can be connected per phase to ACB (MTZ/NT/NW) in BlokSeT?
In new BlokSeT catalogue, we have mentioned the maximum cable size that can be connected per phase of MTZ/NT/NW Masterpact. The cable includes both Copper and Aluminum cables.

For Example, for Side Connection, MTZ2/NW25 breaker, We can connect 2 x 300mm2 copper cables per phase.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: