Search FAQs
Will the M221 support the TM7 IP67 modules?
Issue:
Can the M221 controllers support the TM7 IP67 modules
Product Line:
All M221 Controllers
Environment:
Ecostruxure Machine Expert Basic ( formally SoMachine Basic)
Resolution:
No. The TM7 modules are for the TM258 only. The M221 will support the ETB IP67.
Can the M221 controllers support the TM7 IP67 modules
Product Line:
All M221 Controllers
Environment:
Ecostruxure Machine Expert Basic ( formally SoMachine Basic)
Resolution:
No. The TM7 modules are for the TM258 only. The M221 will support the ETB IP67.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: