{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Why does LTU have some errors when performing automatic tests with LTU and Maintenance Tool on NSX?

LTU has a known limitation when configuring some automatic tests with Maintenance Tool (TRV00911).  This is a result of the pre-setting being different when automatic mode is performed.  As a result, the tests in automatic mode does not have a large enough injected current to trigger the short time protection for some settings.
In this situation, the test will show a false FAIL result.

Example screen shot with failed result:


Workaround: Perform the same testing in manual mode as this uses a different group of settings.
If the same test is done with manual mode, the results will return with a PASS.

Example screen shot with the manual test configuration:



Example screen shot with the manual test test results:

Schneider Electric Saudi Arabia

Attachment(s)

FA305808 LTU Fault on automatic test.pdfFA305808 LTU Fault on automatic test.pdf [271.51 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.