{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What are some of the benefits to the reduction of noise voltages with the Altivar 680/980 Series Variable Frequency Drives?

Issue:
Benefits to the reducing noise voltages with the ATV680/980 drives.

Product Line:
ATV680 ATV980

Environment:
All

Cause:
Benefits of voltage noise

Resolution:
The connection of DC-voltage midpoint with artificial star-point built by filter capacitors will reduce the bearing currents, increasing the lifetime of motor bearings and allows for easy paralleling of power stages.

Schneider Electric Saudi Arabia

Explore more
Range:
MRCA/MRWA Mount - LegacyAltivar Plus Engineered Drives
Explore more
Range:
MRCA/MRWA Mount - LegacyAltivar Plus Engineered Drives
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.