Search FAQs
UL Certificate of Conformity for Harmony HMIGTO series HMI
Issue
Where do I find the UL Certificate of Conformity for Harmony HMIGTO targets and which UL enclosure types are they rated for?
Product Line
Harmony HMIGTO
Environment
Physical characteristics
Resolution
Attached is the UL Certificate of Conformity for Harmony HMIGTO targets.
The HMIGTO series is was tested for UL Enclosure requirements:
Type 1, Type 4X (Indoor use only), and/or Type 13 rated enclosures
Where do I find the UL Certificate of Conformity for Harmony HMIGTO targets and which UL enclosure types are they rated for?
Product Line
Harmony HMIGTO
Environment
Physical characteristics
Resolution
Attached is the UL Certificate of Conformity for Harmony HMIGTO targets.
The HMIGTO series is was tested for UL Enclosure requirements:
Type 1, Type 4X (Indoor use only), and/or Type 13 rated enclosures
Released for:Schneider Electric Saudi Arabia
Attachment(s)
Explore more
Range:
Explore more
Range: