{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Where can I get the minimum resistance and braking resistors for the Altivar 930 and Altivar 950 drives?
Issue:
Selecting a Braking Resistor for the ATV900 Series Drives.

Product line:
Altivar Process Drive (ATV930, ATV950)
note: some ATV960 drives have an ATV930 inside the enclosure so use the ATV930 part number to determine the DB min resistance.

Environment:
Altivar Process Drive

Cause:
n/a

Resolution:
See the attached information from the 06/2022 Installation Manual for the ATV930/950 drives for minimum resistance ratings to match the correct braking resistor.
Using a resistor with lower resistance can result in damage to the drive.
d
Consult the most recent installation manual at this link to ensure this information has not been updated: https://www.se.com/ww/en/download/document/NHA80932/



Schneider Electric Saudi Arabia