{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can the M241 PLC be an Ethernet/IP primary?

Article available in these languages: Japanese

Issue:
Is the M241 PLC an Ethernet/IP primary?

Product Line:
M241, TM241

Resolution:
Starting with SoMachine V4.3,all M241 controllers an Ethernet IP scanner (primary) capability. That includes Machine Expert 1.x and Machine Expert 2.x versions

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: