{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Sepam 80 - saving MET148-2 temperatures to a log file when a protection trips occurs.
As of SFT2841 software version V15.0 and Sepam 80 firmware version V9.01, the temperatures measured by the MET148-2 module are not saved in the Tripping Context of the relay by default.

Please see the attached file for a workaround to this problem.

AEDL3

Schneider Electric Saudi Arabia

Attachment(s)
Sepam 80_Saving_MET148-2_Temperatures_From_Trip_Event_v0.docx [291.36 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.