Do we have interlock option in RM6 to prevent closing of earthing switch onto a live (energized) cable?
RM6 does not offer this interlock feature; as an alternative solution, the use of manual mechanical based key interlocks (catalog page attached) according to the type of cubicle need to be considered.
Released for:Schneider Electric Saudi Arabia
Attachment(s)
RM6_key lock options.pdf [150.61 KB]
Explore more
Range:
RM6
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.