{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
PowerLogic and ION meter default onboard logging configurations

Issue

How to find out what measurements Powerlogic and/or ION meters should be logging by default

Product Line

Power Monitoring Expert 7.2.2
Power Monitoring Expert 8.2
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Power Monitoring Expert 2024

Environment

PM200

PM800

PM5000

ION6200

ION9200

ION9300

ION7300

ION7500

ION7600

ION7700

ION8300

ION8600

PM8000

ION9000

micrologic trip units

Cause

Not all meters use the same templates or have the same default measurement maps for onboard logging

Some meters do not have the capability of onboard logging

Resolution

  • Please find the attached excel document to identify the default logged measurements sorted by device type
    • Set "Logged by Default" to Yes
    • Select the device type you wish to inquire
    • Use the "Row Label" section to view the default measurements

NOTE * If the "Row Labels" portion of the document is blank when "Logged by Default" is set you yes, then the meter does not have onboard logging capabilities and software logging must be configured

Please use article: How to setup PC based logging in the ION Enterprise VIP when a device does not have onboard logging capability. | Schneider Electric USA to help.

Schneider Electric Saudi Arabia

Attachment(s)
How_To_Determine_What_Measurements_Are_Logged_By_Default.xlsx [3.67 MB]