{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How many Magelis HMIs could be connected to the M221 over Modbus/TCP?
Issue:
How many Magelis HMIs could be connected to the M221 over Modbus/TCP?

Product Line:
TM221, Magelis, XBTGK/GT/GH, HMIGTO/GTU/STO/STU, iPC

Resolution:
The M221 controllers that has ethernet can have 8 HMIs communicating to it.  If it is serial, then there is only one Modbus Client.

Schneider Electric Saudi Arabia