Search FAQs
Wire recommendation to use with EM4200 series meters
Issue
Wire recommendation to use with EM4200 series meters
Product Line
EM4200 series meters
EM4235
EM4236
Environment
Meter wiring
Resolution
The EM4200's recommended wire size for I/O, Communications, and CT is 24-16 AWG (0.2 to 1.5 mm2) shielded wire, solid or stranded.
Wire recommendation to use with EM4200 series meters
Product Line
EM4200 series meters
EM4235
EM4236
Environment
Meter wiring
Resolution
The EM4200's recommended wire size for I/O, Communications, and CT is 24-16 AWG (0.2 to 1.5 mm2) shielded wire, solid or stranded.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: