Issue:
Not being able to change motor data settings in the ATV320
Product Line:
Altivar 320
Environment:
All
Cause:
Function blocks are running the back ground you will need to stop the function blocks.
Resolution:
FbM- [FUNCTION BLOCKS] (continued)
FbCd
[FB Command]
Allows to start and stop the function blocks manually.
StOP
Strt
[FB Command] (FbCd) is forced to [Stop] (StOP) if there is no valid function blocks application in the drive memory.
[FB Command] (FbCd) is set to [Start] (Strt) when the function blocks application switch to Run according to
[FB start mode] (FbrM) configuration.
Note: As soon as the function blocks are started, the drive is considered as in running state and the modification of configuration
parameters is no longer possible.
[Stop] (StOP): Function blocks application Stop command
[Start] (Strt): Function blocks application Start command
Not being able to change motor data settings in the ATV320
Product Line:
Altivar 320
Environment:
All
Cause:
Function blocks are running the back ground you will need to stop the function blocks.
Resolution:
FbM- [FUNCTION BLOCKS] (continued)
FbCd
[FB Command]
Allows to start and stop the function blocks manually.
StOP
Strt
[FB Command] (FbCd) is forced to [Stop] (StOP) if there is no valid function blocks application in the drive memory.
[FB Command] (FbCd) is set to [Start] (Strt) when the function blocks application switch to Run according to
[FB start mode] (FbrM) configuration.
Note: As soon as the function blocks are started, the drive is considered as in running state and the modification of configuration
parameters is no longer possible.
[Stop] (StOP): Function blocks application Stop command
[Start] (Strt): Function blocks application Start command
Released for:Schneider Electric Saudi Arabia