Search FAQs
Video: How can the ATV320 be programmed for 2-wire control?
Issue:
ATV320 2-wire control programming
Product Line:
Altivar 320, ATV320
Environment:
All
Cause:
Setup, programming.
Resolution:
From main menu:
If desired, set TCT to LEL instead of TRN for level control.
Warning: Level control type is not appropriate for all applications. Please consider whether this is safe for your application.
-In transition mode (trn), the drive will need to be powered up before a run command is given.
-In level mode (LEL), the run command can remain active, and the drive will run upon power up.
If the run command is not active, the drive will wait for one in RDY status.
ATV320 2-wire control programming
Product Line:
Altivar 320, ATV320
Environment:
All
Cause:
Setup, programming.
Resolution:
From main menu:
- Enter on dial to go to CONF and enter.
- Go down to FULL and enter.
- Go down to I_0- and enter.
- Set TCC for 2C for 2-wire control.
If desired, set TCT to LEL instead of TRN for level control.
Warning: Level control type is not appropriate for all applications. Please consider whether this is safe for your application.
-In transition mode (trn), the drive will need to be powered up before a run command is given.
-In level mode (LEL), the run command can remain active, and the drive will run upon power up.
If the run command is not active, the drive will wait for one in RDY status.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: