Search FAQs
What are the specification on the ATV320 Internal +24Vdc power supply?
Issue:
ATV320 internal +24Vdc power supply specifications.
Product Line:
Drives
Environment::
All
Cause:
Installation / Setup
Resolution:
+24 Vdc, sampling time 2 ms, maximum voltage 30 V, maximum current 100 mA this supply is used for turning on the logic inputs.
Also note that the P24 is not a input for external supply. The P24 is a output supply for the STO safe torque off input.
ATV320 internal +24Vdc power supply specifications.
Product Line:
Drives
Environment::
All
Cause:
Installation / Setup
Resolution:
+24 Vdc, sampling time 2 ms, maximum voltage 30 V, maximum current 100 mA this supply is used for turning on the logic inputs.
Also note that the P24 is not a input for external supply. The P24 is a output supply for the STO safe torque off input.
Released for:Schneider Electric Saudi Arabia
Explore more
Category:
Explore more
Category: