Is there a battery for Real Time Clock in PM2230 energy meter ?
PM2230 has an internal battery to keep its clock running. The life expectancy of the meter’s internal battery is estimated to be over 3 years at 25 °C under typical operating conditions.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
EasyLogic PM2000 series
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.