{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the Short Circuit (AIC) rating for Circuit Breakers inside the ATV660 Drive System?
Issue:
Short Circuit (AIC) rating for Circuit Breakers inside the ATV660 Drive System.

Product Line:
ATV660, Process Drive System

Environment:
All

Cause:
NA

Resolution:
All Altivar 660 Process Drives include a circuit breaker as a disconnect device and
have a short-circuit rating of 100,000 A at up to 480 V.

Schneider Electric Saudi Arabia