{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Do we have braking resistors for the Altivar 600 Process Drives?
Issue:
Braking resistors compatibility with Altivar 600 Process Drives.

Product Line:
Altivar 600 Process Drive (ATV630, ATV650, ATV660, ATV680)

Environment:
All serial numbers for Altivar 600 Process Drive

Cause:
N/A

Resolution:
No, braking resistors cannot be used on the Altivar 600 Process Drive Series.  Braking resistors are only available for the Altivar 900 Process Drives.

Schneider Electric Saudi Arabia