Search FAQs
Error installing PowerChute Business Edition on Linux " rpm failed " and "Please check PCBE is not already installed "
Issue:
PowerChute Business Edition fails to install on Linux with errors " rpm failed " and "Please check PCBE is not already installed "
Product:
PowerChute Business Edition versions 9.2.1, 9.2, 9.1.1, 9.0.4, 9.0.3
Environment:
All supported Linux OS
Cause:
Low hard disk space.
NOTE: The error or errors displayed are incorrect. The error displayed should read "Installation of package pbeagent - 9.0.4 - 401.i 386 requires 95 MB of space (on the / file system)" with the PowerChute version number and space required based on the version being installed.
Required disk space
Solution:
Remove files to increase the available hard disk space or add hard disk space to the system.
PowerChute Business Edition fails to install on Linux with errors " rpm failed " and "Please check PCBE is not already installed "
Product:
PowerChute Business Edition versions 9.2.1, 9.2, 9.1.1, 9.0.4, 9.0.3
Environment:
All supported Linux OS
Cause:
Low hard disk space.
NOTE: The error or errors displayed are incorrect. The error displayed should read "Installation of package pbeagent - 9.0.4 - 401.i 386 requires 95 MB of space (on the / file system)" with the PowerChute version number and space required based on the version being installed.
Required disk space
- PCBE 9.1.1 – 75MB
- PCBE 9.0.3 – 75MB
- PCBE 9.2 – 85MB
- PCBE 9.2.1 – 99MB
- PCBE 9.0.4 – 95MB
Solution:
Remove files to increase the available hard disk space or add hard disk space to the system.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: