{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: How do I add or modify a user in PME?

Issue:
How do I add or modify a user in PME?

Product line:

StruxureWare Power Monitoring Expert 7.01

Power Monitoring Expert 7.2.x

Power Monitoring Expert 8.x

Power Monitoring Expert 9.0

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023



Environment:
Web Application

Cause:
A user's access needs to be revoked or a new user needs to be added.

Resolution:
For SPM 7.01, PME 7.2.x, and PME 8.x

Any changes to user passwords will require a user with Supervisor level access.
Logging into the Management Console with a lower-level account will see the 'User Manager' section grayed out.

  1. Open Management Console
  2. Navigate to Tools > User Manager
  3. Add/remove users and change existing access levels.





For PME 9.0, PME 2020, PME 2021, PME 2022, and PME 2023

3 different types of users are supported - Standard users, Windows users, and Windows groups.
The following table shows the characteristics of each user type:

User TypeCharacteristics
Standard userThis is a PME native user account. The username, password, and
details are defined in the PME User Manager.
Windows userThis is an account from an external Windows system. The
username, password, and details are defined through the Windows
Active Directory or local Windows operating system.
Windows groupThis is a group of accounts from an external Windows system. The
username, password, and details are defined through the Windows
Active Directory or local Windows operating system.


Any changes to user passwords will require a user with Supervisor level access.
There are two methods to access User Manager:

From Management Console:

  1. Open Management Console
  2. Select User Manager under Tools > Web Tools

It will direct you to User Manager in Web Applications

From Web Applications:

  1. Open Web applications
  2. Go to Settings > Configuration Tools > User Manager

Schneider Electric Saudi Arabia