Issue:
Availability of lugs as a replacement part for high horsepower ATV600 / ATV900 series Process Drives
Product Line:
ATV6xx, ATV9xx
Environment:
All
Cause:
Customer needs to install or replace lugs
Resolution:
We do not offer lugs for the ATV600/ ATV900 series drives. Bare terminals are available on the drive so that the customer can best choose the lugs to match the wiring they are using. We would suggest contacting Thomas & Betts, Burndy or Illsco for lugs.
The open style ATV6XX and/or ATV9XX has ring terminals that indicates that lug kits do not come with the high horse power units.
If it's ordered as part of an ATV660 enclosure, MCC package or Altivar outdoor they would probably be included, but not with an open style Drive that has a high horse power rating.
Released for:Schneider Electric Saudi Arabia