Issue:
I want to implement the M580 with DRS Architecture.
Which ConneXium DRS switches can be used with M580 Remote I/O offer?
Product Line:
M580
Connexium Switch
Environment:
EcoStruxure Control Expert
Internet Explorer
Resolution:
The Dual Ring Switches (DRS) that can be implemented with M580 Remote I/O to extend the performance of the architecture are the following:
I want to implement the M580 with DRS Architecture.
Which ConneXium DRS switches can be used with M580 Remote I/O offer?
Product Line:
M580
Connexium Switch
Environment:
EcoStruxure Control Expert
Internet Explorer
Resolution:
The Dual Ring Switches (DRS) that can be implemented with M580 Remote I/O to extend the performance of the architecture are the following:
- TCSESM083F23F1 (8TX 1280) : 8 COPPER PORTS
- TCSESM063F2CU1 (6TX/2FX-MM) : 2 multi-mode fiber ports + 6 copper ports
- TCSESM063F2CS1 (6TX/2FX-SM) : 2 single-mode fiber ports + 6 copper ports
Released for:Schneider Electric Saudi Arabia