{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
STB IO - why the STBACO1210 doesn't work if two sensors are connected with internal power supply mode
Question:
why the STBACO1210 doesn't work if two sensors are connected with internal power supply mode

Answer:
For STBACO1210,the two output channels are none isolated and you could choose one these options:
1, use external isolated DC power supply to each channel.

2. if use internal power supply, you can only use one channel to wire sensor (another channel as spare)

Schneider Electric Saudi Arabia