undefined [object Object]
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do we change the color of a Vijeo Designer Toolchest image from the image library?
Issue:
Is it possible to change the color of a Vijeo Designer Toolchest images from the image library?

Product Line:
Vijeo Designer (all versions)

Resolution:
Today the easiest way to change the colors of any toolchest images from the image libraries is to use this procedure:
1) Drag the desired image on to your Vijeo Designer Panel
2) Select the image and then Copy (Ctrl + C)
3) Open Microsoft word and Paste (Ctrl + V)
4) Select the image in Microsoft word and then Copy (Ctrl + C)
5) Open Microsoft Paint and Paste (Ctrl + V)
6) Use the Color Filler to change the colors of the image
7) Once you are done, select the image and Copy/Paste into Microsoft Word again
8) Copy/Paste from Word to Vijeo Designer
9) In Vijeo Designer, enable the Anti-Alaising and set the transparent color to be the back ground color of the image.

Schneider Electric Saudi Arabia