Issue:
Can I synchronize the M580 PLC clock by BMENOC0301/11 NTP service ?
Product Line:
M580
Environment:
EcoStruxure Control Expert
Resolution:
In order for the time on the CPU module to synchronize with the BMENOC NTP service, you need to enable the network time service, in the DTM browser of the BMENOC, ,then select the checkbox "Update CPU time with this module".
The project will need to be built and downloaded to the CPU.
Released for:Schneider Electric Saudi Arabia