{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What upgrades were made to firmware version 8.09 for a Connexium TCSESM series switch?
Issue
A change was made to the TCSESM series switch firmware to fix an SNMPV3 authentication vulnerability.


Product Line
The Connexium products affected by this vulnerability with version 8.04 or lower are:

TCSESM043F23F0TCSESM103F23G0TCSESM063F2CU1C
TCSESM043F1CU0TCSESM103F2LG0TCSESM063F2CS1C
TCSESM043F2CU0TCSESM163F23F0
TCSESM043F1CS0TCSESM163F2CU0
TCSESM043F2CS0TCSESM163F2CS0
TCSESM083F23F0TCSESM243F2CU0
TCSESM083F1CU0TCSESM083F23F1
TCSESN083F2CU0TCSESM063F2CU1
TCSESM083F1CS0TCSESM063F2CS1
TCSESM083F2CS0TCSESM083F23F1C

















Resolution
The implementation of SNMPv3 contains a vulnerability that may allow authentication bypass if specifically, crafted packets are used.
To resolve this vulnerability, upgrade the Connexium switch to V8.09 or greater.

Schneider Electric Saudi Arabia