{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do you change the motor rotation on the ATV630 or ATV930 Process Drives?
Issue:
ATV630 or ATV930 Process Drives requires to change the motor rotation.

Product Line:
Altivar Process Drives

Environment
All

Cause:
Wants to change the motor's rotation

Resolution:
From the Main menu:
Select Complete settings
Select Motor parameter settings
Select Motor control
Select Output phase rotation
Factory default is ABC. This can be changed to ACB.

Schneider Electric Saudi Arabia