{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for a key to the floor mounted ATV660 door handle?
Issue:
Key for the floor mounted ATV660 door handle.

Product Line:
ATV660, Altivar 660

Environment:
Floor mounted enclosures

Cause:
Need replacement key

Resolution:
The ATV660 door has a lockable handle.  The door handle key for the floor mount enclosure is part# NSYLDB5.
https://www.se.com/ww/en/product/NSYLDB5/metal-key-for-5mm-double-bar-insert/

Picture of Key Handle for locking door panel

Schneider Electric Saudi Arabia