{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for the DeviceNet Fieldbus Module for the Altivar Process Drive?
Issue:
What is the part number for the DeviceNet Fieldbus Module for the Altivar Process Drive?

Product Line:
Altivar Machines, Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)

Environment:
All serial numbers for Altivar Process Drive

Cause:
Part number required to order part

Resolution:
Altivar 600/900 Series
Part Number - VW3A3609

Schneider Electric Saudi Arabia