{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
CM4000 rebooting intermittently
Issue
CM4000 meter reboots itself intermittently.

Product Line
CM4000, CM4000T

Cause
Sending an IRIG-B time synch signal (instead of a DCF-77 format signal) into a digital input configured for time synch on the CM4000 causes it to reboot randomly.

Resolution
Ensure that the proper I/O format signal is connected to the CM4000.
The CM4000's can only accept DCF-77 time synch signals.

Kindly refer to page 72 of the CM4000 Reference Manual for more details on time synch signals.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.