{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Video: Wiring & Programming Status Relays R1 & R2 on the ATV320 Drive

Article available in these languages: Finnish

Issue:
How are the relays for ATV320 drive programmed?

Product Line:
Altivar 320

Cause:
Relay programming.

Resolution:
2 relays available: R1 and R2.
R1 can be wired as normally-open (R1A and R1C) or normally-closed (R1B and R1C).
R2 is normally-open only.

To program relays:
Enter and scroll down to CONF.
Enter and scroll down to FULL.
Enter and scroll down to I-O menu.
Enter and scroll down to R1- or R2- depending on preference.

See attachment for relay programming, relay delay time, relay active at, holding time, and relay fall back assignments.

Schneider Electric Saudi Arabia

Attachment(s)

ATV320 relay programming.pdfATV320 relay programming.pdf [159.12 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: