{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: How do we display the username of the operator who ACK'd an Alarm in Vijeo Designer?
Issue:
Is there a way to track the operator's username who acknowledges and alarm on the HMI?

Product Line:
Vijeo Designer (all versions)

Resolution:
In order to display the username of an operator who ACK'd an Alarm in Vijeo Designer, there are a few things that need to be set up in the application.

1) First, Target Security needs to be activated and you should have at least one Security Group and one User defined.
2) You will need to have Alarm variables defined in your AlarmGroup and should have an Alarm Summary object on one of your panels.
3) In the Alarm Summary, you should add the column "Username" in order to have a place to show the information.
4) Under the "Alarms & Events" node, you will need to activate the "Track User in Alarms" property. Set it to "Yes"

With this configuration, whenever an alarm is ACK'd, the username column will be populated with the operator's username.

Schneider Electric Saudi Arabia