Search FAQs
On the ATV630 and ATV930 process drives, why can't the digital input assignments be changed?
Issue: ATV630/ATV930 the digital input assignments are not changing in the Input/Output menu? Product Line: Altivar Process, Altivar 630, ATV630, Altivar 930, ATV930 Environment: All models Cause: Attempting to change DIx assignments in the COMPLETE SETTINGS > INPUT/OUTPUT menu Resolution: The digital input assignments in the INPUT/OUTPUT menu are read only. To change an assignment, you need to go to the desired function and then assign an Input to the function. Example: to assign Reverse to DI2, you need to go to "Reverse assign" in the Command and Reference menu, and change that to DI2. Link to the ATV600 programming manual: https://download.schneider-electric.com/files?p_Doc_Ref=EAV64318 Link to the ATV900 programming manual; https://www.se.com/us/en/download/document/NHA80757/ |
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: