Masterpact NW ACBs comply with IEC 60947-2. Temperature rise tests for Masterpact NW ACBs are specified in standard IEC 60947-2. Please find attached a declaration of conformity illustrating the maximum allowable temperature on the terminals of the Masterpact NW ACB.